This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3436: LVDS Interface on FPGA (XC7Z020- 1CLG484I4493)

Part Number: DLPC3436


if we understand correctly, the AP needs two LVDS ports to connect to FPGA in order to driver 1080p. The reason is that the standard LVDS interface supports 85Mhz clock (if I understand it correctly).

The AP we may choose to use however supports only one LVDS port (with 148.5MHz clock).

I wander if it is possible for FPGA to support single LVDS with higher clock frequency (148.5MHz).

If not, how might be alternative solution? to use a 1 to 2 bridge? or we may have to use RGB interface, which is less interference free.