Other Parts Discussed in Thread: DLP2010,
Dear All,
I am using DLP2010 and DLP2010NIR for my research. I found from your webpage handy document "DMD Optical Efficiency for Visible Wavelengths" https://www.ti.com/lit/an/dlpa083a/dlpa083a.pdf. On the 13th page of the material is a Figure 4-6. 5.4 µm Pitch DMD Mirror Calculated Diffraction Efficiency, for the wavelength range from 400nm to 700nm.
I am wondering what is the DMD Mirror Calculated Diffraction Efficiency in the range from 350nm till 750nm. Could you please provide any information about the behaviour of the DMD for the mentioned range?
I was also searching that type of document for the DLP2010NIR, but unfortunately I could not find. If you have, could you please provide diffraction efficiency plot or numerical data for the DLP2010NIR?
Thank you in advance.
Best regards,
Astghik