Other Parts Discussed in Thread: DLPA2000, , DLPC3430, DLPC3435
Hi,
Our current setup is a third-party projector using a DLP2010 DMD, being driven by the TI LightCrafter EVM (DLPDLCR2010EVM, using DLPC3435, DLPA2010 chip-set). The projector is connected to the LightCrafter with a customer connector. We've also been able to reproduce the issue in another setup, using our own hardware, which use the DLPC3430, and DLPA2000 chip-set (which do not use the custom connector I previously mentioned).
The issue is that when we continually re-power / reset the device we are seeing a missing column of data, and the image is shifted but still in the correct order. When we change the image, this artifact remains.
I've included two pictures, from the Lightcrafter setup. The first picture is the correct test pattern, which was shown on reset. The second image is the what was displayed when we reset again. The issue does not occur all the time. It takes several resets to reproduce the issue.
Please let me know if you have any questions, or if there is any more information that I can provide.
Thank you very much for your time.
Kind Regards,
Stephen Craig
Design Engineer
Avalon Holographics
stephen.craig@avalonholographics.com
Correct Test Pattern