This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3478: How to rewrite splash pattern data during operation

Part Number: DLPC3478
Other Parts Discussed in Thread: DLP3010EVM-LC

Nice to meet you
My name is Tak.

I am evaluating the DLP3010EVM-LC now.


The purpose is to rewrite the 1280 x 720 splash pattern data for 2 planes while the EVM is operating.

Set "Write Flash Data Type Select" to "0x90-OEM Splash Screens" in advanced mode of GUI tool
Is it possible to set and rewrite the splash pattern data?
Also, how should the splash pattern data prepared for that be created?
I think compression of splash pattern data is also necessary, so can you tell me the data format?

Thank you.