Other Parts Discussed in Thread: DRA71XEVM, DRV8889-Q1EVM
Hello Guys,
Good day!
We have a customer looking to develop a Heads-up display using the following EVMs:
- PGU unit – DLP3030-Q1 EVM
- Application processor – DRA71xEVM
- Motor driver -- DRV8889-Q1EVM
They have a list of questions which were hoping you can help us with.
1. Do we get a reference codes (like driver codes, Application codes, utility tools etc.) for the testing of the heads-up display design?
2. What software and hardware tools do you recommend procuring in order to achieve our goal?
3. What is the difference between the DRA71xEVM CPU board and JAMR3 Tuner application board? Which is suitable for the HUD application as an application processor?
4. Is the hardware mention above for the application processor requires Linux based development? If there are different ways which one do you recommend for the development?
5. Any recommended automotive camera modules that are suitable for application processor?
6. Is it possible to buy or lease a sample boards for certain amount of duration? If yes what will be the process?
Thanks in advance!
Art