Other Parts Discussed in Thread: DLPC910, , TIDA-00570, DLPC900, DLP9000
I am planning to take up a projector project and wish to use your product DLP9000X. When I gone through datasheet of DLP9000X, it is understood that DLP9000X should be used with DLPC910 controller. It was also noted that interface between DLPC910 and host processor is documented properly. But I am planning to use DLP9000X with my custom board in which Virtex 7 ultra scale FPGA is present. Hence, I would like to connect my virtex 7 FPGA to DLP9000X without DLPC910. In this case, I need interface requirement details of DMD DLP9000X. If you can share the details, I can capture requirements of DMD DLP9000X and this will assist in planning my project requirements.
Anticipating your affirmative response,
regards,
M Muthukumar