This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPNIRNANOEVM: DLPNIRNANOEVM

Part Number: DLPNIRNANOEVM


Hello,

we need a fully automated installation (silent installation) because our users do not have to intervene in the installation and we do the maintenance work even at night when no user is sitting at the PC.

Currently I am starting the installation like:
 

DLPNIRscanNanoGUI-2.1.0-windows-installer.exe  --unattendedmodeui minimal --mode unattended  --debugtrace "C:\WINDOWS\TEMP\DLPNIRscanNanoGUI.2.1.0.18.05.2020.Install.log"


Nevertheless, dialogues are displayed which must be confirmed. This is not feasible if, for example, the user is not sitting at the PC - so all our maintenance scripts would abort. Is there an other way to solve this?

Please send your answer also to our IT-specialists ticket@dbfz.de.

Best regards

Jana Mühlenberg

jana.muehlenberg@dbfz.de