Part Number: DLPLCR9000EVM
Hi,
I'm testing a DLPLCR9000EVM(DLP9000 EVM) kit.
When I connected the kit to a PC with an USB connector, then power up.
I can find that the LEDs of D5, D11 & D12 lighted up green (it means that power is normal)
but, unfortunately, next the LEDs of D7 & D9 did not turn on, as following picture. (It means that the DLPC900 was not operating normally.)
Also, DMD showed a strange & halt pattern, as following picture. It did not show any more changed images.
So, I tried to find a connection(USB) in device manager of windows 10 PC, but It was not appeared anywhere...
(Maybe I think a EVM kit was not connected correctly to the PC or DLPC900 was break down....)
Finally, I tried to reload/upload a firmware (ver. 5.0.1) to the kit via DLP LCR6500 & LCR9000 GUI S/W, but, I faced an error, as following pictures,
I tried to following discussion (DLP9000: LightCrafter 6500 & 9000 - 4.0.1: Error on uploading firmware file & Error on image display), but it did not resolved, same phenomenon....
So, how can I save(?) that kit, like reloading a firmware, checking whether DLPC900 is live or dead, whether DMD was break down, and so on...