This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPNIRNANOEVM: DLPNIRNANOEVM

Part Number: DLPNIRNANOEVM


Seeking information on optical coupling of a fiber to a NIRscan Nano EVM. I assume that I will remove the supplied window and replace it with a collimating lens and optical mount to couple light from the lamps into the fiber end. I can also choose not to use the lamps inside the Nano EVM and instead use an external light source that couples transmitted or reflected NIR into the fiber that is then dispersed onto the grating. I do not see any means for mechanically mounting a fiber onto the NanoEVM, but see a recent post in which this seems to be the case. Any assistance would be greatly appreciated.

Paul