This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCRC410EVM: 64 bit version of the dll - D4100_usb.dll

Part Number: DLPLCRC410EVM

Hi Team,

Good day.

My customer is looking for the 64-bit version of the dll - D4100_usb.dll, do we have this one? 

His application (that includes other components too) needs to be a 64-bit application as other components including the platform is 64 bit. He needs a 64bit to use to incorporate into the software so that there is compatibility.

Thanks in advance.

Regards,

Renan

  • Hello Renan,

    The GUI is built on the 32 bit version, which the 64 bit Windows OS can use.  There is no 64 bit version as far as I am aware.

    The software is intended for test purposes and not production for this controller.

    Fizix