Hello,
Actually, we have a problem on the timing lock issue. In our system, the front-end IC converter the VGA analog signal and output to TI’s scaler(ex: DDPxxx). When input a standard XGA(1024x768-60Hz) timing, we found the DDP will wrong detect it as a interlaced signal shown in the TI’s DLP composer tool. Of course, the system can’t lock the signal correctly.
Is there anyone can help to explain the meaning of H-sync pulse count in V-Sync width? Will TI’s autolock algorithm use this information to calculate and determine the input timing resolution? What’s the possible root cause of this problem? Thanks.