Hello,
We are considering purchase of lightcommander to couple its light-engine with a microscope. The key requirement is that the output of the illumination module be of (more or less) uniform intensity and uniform angular distribution at the output. For me to judge the properties of the output light, is it possible to have a schematic of the optical arrangement of the core optics module and illumination module? For example, I am wondering how the non-uniform light from LED is made homogeneous? Does Lightcommander use integration rod and TIR prism?
A secondary question related to the above:
The video http://e2e.ti.com/videos/m/dlp_mems/240437.aspx helpfully describes that one can combine the illumination module, power supply and control module on an optical bench. With that much hardware, can one connect an HDMI input to drive the DMD? Will that hardware be controllable with logicPD software?
And a tertiary question:
What are (ballpark) dimensions and weight of the light-engine and control board once mounted on the optical bench?
Thank you
Shalin