This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3000-C300REF: DLP3000

Part Number: DLP3000-C300REF

Hello,

I want to create diagonal straight lines using DLP3000 by uploading a binary image (pixels are square-shaped). I want to ask two questions. 

1. DLP3000 is designed as diamond-shaped mirrors and it is sometimes hard to generate straight lines using these mirrors. Assume that I want to create a diagonal line as shown in the figure below. The first pixel - which should be 'one' or ''on' - is Row_0 & Col_0 on the binary image (which will be uploaded). The third pixel is Row_2 & Col_1. My question is that what is the intermediate pixel between the first and third pixels. Is it Row_1 & Col_0 OR Row_1 & Col_1 OR just Empty/Null?

2. My second question is about corresponding pixels and mirrors. Row_0 & Col_0 pixels start at the top left on a usual image, but the DLP3000 starts from top right. What kind of binary image I need to upload. I mean if I want to turn on the Row_0 & Col_0 mirror, do I need to make '1' for Row_0 & Col_607 pixel on the binary image?

Thank you for your answer.

Batu

photo.tif