Hi
Mayank,
I still evaluate the DLP3010EVM-LC,
Using Internal Pattern Mode (Trigger In Mode),
The Exposure Time was re-evaluated up to 2 seconds.
As a result of detailed evaluation, when Exposure Time exceeds 800 ms
I ran into a strange problem.
Please see the table below.
When ExposureTime is 800ms or more
There is a difference in the timing of Pre Dark Time and Trigger Out 2
I found out.
As a result, the timing of LED lighting and the output timing of Trigger Out2
It seems that they are out of alignment.
In addition, as the Exposure Time becomes longer, the actual pattern becomes a fixed cycle.
I also confirmed that the display is changing.
I believe you will solve this problem.
First of all, would you like to see something similar happen in your environment?
Thanks and regards,
Tak