Other Parts Discussed in Thread: TM4C1297NCZAD
This question is regarding the DLP® NIRscan™ Nano Evaluation Module
I am looking at DLPNIRscanNanoSoftware v2.1.0 (un-modified TI distribution) and trying to determine where the timer callback function TimerIntHandler() is set to be the interrupt handler callback for TIMER0 (TIMER0_BASE). I am not able to locate this association. Searching the TI Support Forums pointed me to the board specific _startup_ccs.c file (e.g. tm4c1297nczad_startup_ccs.c). That looks like the right place but this file isn’t part of the project and there is no association in that file for TIMER0.
#pragma DATA_SECTION(g_pfnVectors, ".intvecs")
void (* const g_pfnVectors[])(void) =
{
(void (*)(void))((uint32_t)&__STACK_TOP),
// The initial stack pointer
ResetISR, // The reset handler
NmiSR, // The NMI handler
//…
IntDefaultHandler, // Timer 0 subtimer A
IntDefaultHandler, // Timer 0 subtimer B
IntDefaultHandler, // Timer 1 subtimer A
IntDefaultHandler, // Timer 1 subtimer B
// …
IntDefaultHandler, // Fan 1
0, // Reserved
};
Any idea where the function TimerIntHandler() gets assigned to be the callback function for TIMER0?