Part Number: DLPLCRDC4422EVM
Hello,
I am going to design the 4K UHD projector using DLPLCRDC4422EVM and DLP660TEEVM.
I have searched for the front end board which will be connected with the DLPLCRDC4422EVM but not found.
I need the help to select the Front End Board which has HDMI and other basic Input interface and connect with the DLPLCRDC4422EVM Board.
Also suggested light source compatible with this set up.
Kindly suggest the best options for the front end board for DLPLCRDC4422EVM.
Regards,
Alpesh.