Part Number: DLPLCR9000EVM
Hi,
We want to upload images (bit depth 1) on the DMD which cannot be compressed using RLE or ERLE because they consist of "single pixel structures". For testing we just used video or video pattern mode but in the end we do not want to be limited by the 120 Hz pattern rate. The pattern on the fly mode fits perfectly well but it takes very long to upload patterns which cannot be compressed. That is why I am wondering if it would be possible to upload images using HDMI (in the pattern on the fly mode).
Is there a way to do this?