Other Parts Discussed in Thread: TIDA-01474, DLP470NE, DLPC3470
Dear TI support
Hello.
I'm looking for a DLP device with high response speed.
I read this document (TI Designs: TIDA-01474) which says DLP470NE runs 120Hz with 1-frame latency.
I also see that DLP2010EVM-LC is designed for high-speed applications.
Can you tell me which has less input lag?
I want to reduce the amount of time it takes for input signal to be displayed on the screen.
Thank you.
Kawakami