This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2010EVM-LC: Flash IC and firmware

Part Number: DLP2010EVM-LC


Hello TI,

I'm working with the DLP2010EVM-LC and would like to place a different Flash IC on the EVM or on a daughter PCB.

The EVM uses a MX25L6473EZNI-10G and the one I would like to place is a W25Q64JVSSIQE.

Will this work without any alteration to the firmware?

Also, do I need to load the firmware on to the new Flash IC before soldering it, or can I load the firmware on to the new Flash IC through the DLP-GUI, just like a firmware update?

Kind regards,

Job