Hi everyone,
We have both the NIRscan Nano (900-1700nm) and the NIRscan EVM (1350-2390nm) in our lab. Using a transmission measurement and the Optecks transmission module for the Nano - can I extend my NIR spectrum from 900 to 2390nm by simply combing both CSV files from the Nano and high performance EVM?
Although I'm sure I can simply paste the values from one file into another (ie. combine CSV file) - I'm not sure if I need to take into consideration alignment issues due to the different optics in both spectrometers.