Part Number: DLP2010EVM-LC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DLP2010EVM-LC
Martti,
The main difference between the DLP2010 and DLP2010-LC is that the DLP2010-LC has additional features to support light control applications, such as 3D printing and 3D scanning using both internal and external pattern streaming. The DLP2010 EVM only supports display applications. Note that the DLP2010-LC can be used in display mode as well.
DLP2010 EVM has a DLPC343x controller: https://www.ti.com/lit/ds/symlink/dlpc3430.pdf
DLP2010-LC EVM has a DLPC347x controller: https://www.ti.com/lit/ds/dlps110b/dlps110b.pdf
You should consider the DLP2010-LC EVM if you are interested in the above applications.
I hope this helps.
Regards,
Philippe Dollo