This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR4710EVM-G2: DLPDLCR4710EVM-G2

Part Number: DLPDLCR4710EVM-G2

Hello. I have downloaded the firmware for DLP4710EVM-Q2 ver. 770, but when I try to upload it to the LightCrafter DLP LightCrafter software sas this wirmware mean for different EVM. Wat is wrong?

  • Yuri,

    This is a known issue when using Firmware builds downloaded from the firmware selector tool (which are intended for use with custom boards employing the appropriate DLP chipset). We are looking into this issue, though for now you should use the firmware available on the EVM tool folder to avoid this incompatibility:

    Regards,

    Philippe Dollo