This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR4500EVM: LED datasheets and orientation of the optical systems planes

Part Number: DLPLCR4500EVM


Hi team,

Can you answer a couple of my customers questions?

- Which blue and green LEDs are built into the LightCrafter. (the data sheets would be good) At which of the LED positions are blue and green?
- Is a Scheimpflug - arrangement realized in the construction? And if so with which angles and distances?

Thank you,

Franz

  • Hi Franz,

    The iView IPD 1231 light engine is used in the DLPLCR4500EVM. Since it is sourced from a third party, the specifications and other technical information will have to be requested from iView Limited. Their contact information can be found here

    Thank you,

    Chris

  • Hello Franz,

    Please refer to the following thread on this subject. It has the information you are looking for on LED.

    https://e2e.ti.com/support/dlp/f/94/p/708807/2612953  

    There is no Scheimpflug - arrangement used in any of our EVM optical engine.

    regards,

    Vivek