This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP9500: Response time

Part Number: DLP9500

Hi team,

Good day.

Our customer is controlling the DLP9500  together with DLPCRC410EVM using Labview. The image took ~5secs to load and they would like to modify the response time to load multiple images faster. Is it possible to reduce the response time to 2s?

Regards,
Carlo

  • Carlo,

    This is very dependent on several factors. 

    The speed of their computer, and the USB speed.  However, 5 secs seems a little long.

    Are they using the ActiveX layer or the DLL directly.  Using the DLL functions directly usually speeds things up a little bit.

    Also, I do not know how they are doing the load.

    Fizix