This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP5534PROJQ1EVM: How do I set the source to HDMI immediately from power up?

Part Number: DLP5534PROJQ1EVM

I'm working with the DLP5534PROJQ1EVM Evaluation Module and am trying to figure out a way to have it source from the HDMI input immediately upon power up. Right now, it defaults to the TI DLP splash screen, and I have to use the DLPC230 Control Program to select the source every time power is applied. I'd like to set it to HDMI input by default and not have to use the Cheetah SPI for demonstration purposes.

Many thanks in advance!