This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2010EVM-LC: Vertical Offset of the projection and trigger In functionality

Part Number: DLP2010EVM-LC

Good Morning,

 

I have some questions regarding the DLP2010EVM-LC.

First of allI was wondering what the  vertical offset of the DLP is?

 

I was not able to find this in the datasheets and guides.

If it is not clear you can see in the picture below what i mean by offset.

 

 

 And is it possible to somehow adjust the offset?

 

My second question is if there is any way to use the “trigger in” functionality outside of internal pattern streaming mode?

 If I understood correctly it is exclusively made for that mode but I just wanted to make sure that there is no way to start displaying video via hdmi using some kind of “trigger in” signal.

 

Thank you in advance,

 

Cyrill