This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Development Kit for Beam Shaping

Other Parts Discussed in Thread: DLPDLCR2000EVM, DLP2000, DLP3010EVM-LC

Hello everyone, 

my name is Chris and I am trying to find the right development kit for my purpose.

I hope that someone could help me a little bit because my experience in the area of DMDs is small. 

We want to use a laser ( ~ 10 mW or higher) and shoot with it on a DMD. With the DMD we want to control the shape of the light to create arbitrary light patterns. I tried to find the right development kit for our little project. But at the end I am not sure what is the right choice. 

I realized that the Kits DLPDLCR2000EVM and DLP3010EVM-LC are not the right ones because they work with an additional light engine which can not be removed. I also read in the forum that the DLP2000 is the wrong DMD for lasers but I couldn't find the reason for that. (Maybe because the power from a laser is too high?)

I would be happy if someone can help me a little bit.

That is my first message in this forum. Please inform me, if I my question is inappropriate or when I'm in the false forum.

Best regards

Chris