This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500: Upload and display bitmap images?

Part Number: DLP4500
Other Parts Discussed in Thread: DLPC350

Hello,

What is the recommended way to upload a bit depth = 1 image to the DMD of the DLP4500EVM over usb? For example, the DM365 chip of the LightCrafter3000EVM has the "Static Image" command (see DM365CommandInterfaceGuide, DLPU007D), and the DLP6500 has a "pattern-on-the-fly " mode, where bitmap images can be uploaded over usb. Is there an analogous function for the DLP4500?

Thanks in advance!

- Matt