Other Parts Discussed in Thread: DLP650LNIR
Hello.
I would like to design a laser light source projector to create a structured lighting system.
(1) Is there an optical system that is an example of a laser light source?
(2) Is there a difference between telecentric and non-telecentric depending on the presence or absence of a prism in the optical system of the DLP™ system, and does it affect the laser source, such as interference from DN2509927?
If it is a simple design, there is no need to put in a prism.
(3) If a prism is needed, I would like to know if there is a prism that fits the DLP650LNIR.
Thank you for your help.