This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2010EVM-LC: DLPDLCR2000EVM or DLP2010EVM-LC

Part Number: DLP2010EVM-LC

Hello, I wonder if DLPDLCR2000EVM or DLP2010EVM-LC can be synchronized with a camera by receiving or send a trigger signal?

In general I would like to do a similar thing in the link in your next email for DLP2010EVM-LC: Project a pattern and trigger a camera to capture that. Which way works better/easier, DLPDLCR2000EVM+ Beaglebone Black or DLP2010EVM-LC (more expensive)?

I think Beaglebone Black can send trigger signal to a camera, but how does the Beaglebone Black control the DLPDLCR2000EVM? Is it the case that my PC displays an image then the image is transferred to the DMD by Beaglebone Black through USB or HDMI? But how does the image update on the DMD will send out trigger signal? Is it possible to pre-store a few images in the Beaglebone Black and let it update the image on the DMD sequentially and sends out trigger signal? What is the max frame rate it can be achieved? 

How about the DLP2010EVM-LC? Does it have a standalone control and trigger sending mechanism? 

Thank you very much!