Dear all:
I am trying to use DLP1700 for longer wavelengths application. Simulations showed it should work for NIR and MIR.
I also acknowledged that the transmission window is coated with some material to reject energy outside the frequency range. For DLP1700, the wavelength should not be larger than 2.5 microns in order to get a acceptable transmission through the window.
The problem is that, since I cannot remove the window which protect the DMD , is it coated for a single side of the window or both sides? Can I just scratch the coated material from the window and design a new filter for my application?
Best wishes
Jack