Hello,
I could find RESERVED_ pins in DLP9500 reference schematic(DLP012A-001_SCH.pdf). Where is the descriptions?
Regards,
Uryyy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Uryyy,
You are correct, the six reserved pins listed on page 12 of the current DLP9500 data sheet ( DLPS025E) do not show up in the schematic. I have rev B of the schematic but it is the same and does not contain these pins.
This will take some inquiry to our DMD team.
Fizix
Hello Uryyy,
It appears that these were not included in the design to accommodate the thermal interface, but these are not to be used by end customers and should be left unconnected. However, the pads on the DMD should not connect with any electrical signal, including ground.
We are looking at including these in the pin table of the DMD data sheet.
Fizix