Other Parts Discussed in Thread: DLPC3479,
Hi,
I have a few question about the temperature acquisition command.
(1) Is the temperature calculated using the B constant of the thermistor?
(2) What is the temperature range of the B constant you are using for temperature calculation?
Also, how does the DLPC3479 behave when the thermistor exceeds that temperature range?
(3) Is it possible to change the FW of the DLPC3479 if I want to use a thermistor with a different B constant than the one installed in the EVM?
Regards,
Goto