Hello,
We use DLPA3005 to drive the LEDs.
The current value is set by the register of IDAC [0: 9],
but it has been confirmed that a difference of about 200mA occurs between the units even with the same setting value.
Is this difference dependent on the IC?
And, how much is the current value error designed to be within?
The following are the set values and the measured current.
-Feedback shunt resistance is 9 mΩ (allowable value 1%).
-Only DRIVER A is used.