Other Parts Discussed in Thread: DLPC2607, , DLPC3470, DLP2010
Hi, I'm working with a project that wants to use the micromirrors to dynamically display a pattern sequence, but I cannot find a detailed description of either the high speed or the low-speed interface protocol. Could someone tell me where to find those protocols?
I find that most of the solutions use the DLPC2607 but we find it not suitable for our project, and we prefer to use a very small CPLD to communicate with the DLP2000 directly.
A brief description of our project:
1. We try to build a very compact device that can project mono-color laser patterns so that we would use as few components as possible for keeping it small.
2. We use a mono-color laser as the light source and only project binary 0-1 patterns, but want a high refresh frequency, so it seems that the Parallel I/F of 24 bit RGB on DLPC2607 is redundant in our project.
3. We need to produce a sync signal for triggering other devices when a new frame is projected, we decided to communicate with the DLP2000 with a CPLD and output the trigger pulse from that
4. The pattern sequence is pre-designed and we decided to load it from the built-in FLASH memory inside the CPLD.