This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500: DLP image issues

Part Number: DLP4500

I`m Ji-Nam Park , a sales department team of UniOTech in south Korea

it`s nice to working with you.

My customer is currently testing using DLP4500AFQD. 

They made images by shooing RGB Laser into DLP.

However , the image of the DLP pixel is simultaneously visible to the image of laser , shown in the picture above.

what is the current problem that makes the image visible at the same time?

they want the image like the picture below to be check.

i would grateful appreciate it if you check and let me know. 

i hope for your answer.

Thank you.

Best Regards,

Ji-nam Park

 


UniOTech Corp. (Unique Optical Technology)
Address : B313, 17, Techno 4-ro, Yuseong-gu, Daejeon, Republic of Korea, postal code 34013
Tel : +82-42-933-9870~1 / Fax : +82-303-0959-9870 / Mobile : +82-10-5045-9495
Ji-nam Park/ Assistant manager / Website : http://www.uniotech.kr / E-mail : jinam@uniotech.kr
LASER, VCSEL, DETECTOR, LASER DRIVER, SCANNER, LENS & CRYSTAL, DOE & BEAM SHAPER, FIBER OPTIC, 광학설계, 모듈 제작 양산, 프로그램 제작

  • Hello Ji-nam,

    Welcome to the E2E forum and thank you for your interest in DLP technology.

    Is your client using the DLPDLCR4500EVM or a custom board? How was the below image obtained? Was this on a different system?

    Regards,

    Austin

  • Dear Austin.

     

    Thank you for answer.

    My customer uses the same product as DLPDLC45000EVM for control board and projection lens.

    Other than that , optical system was designed by them.

    Why is the pixel visible only on my customer designed system?

    Could you please check it?

    If possible , could you please provide to me the solution?

    I would grateful appreciate it if you check and let me know

  • Hi Ji-Nam,

    Is your customer using a direct laser or LEDs on the DMD in the custom optical engine?

    Does your client care more about the color balance or the diamond shapes appearing?

    Regards,

    Austin

  • Dear Austin.

    my customer cares about both things.( color balance and Diamond shapes ).

    they want to diamond shapes to be invisible and color not separated from the boundary.

    and they are input laser through TIR Prism into DMD. 

    Ther understand that the color is separated from boundary because of the dispersion , but they do not understand that the diamond shape is visible.

    if possible , could you please guide me to the cause and solution? 

    i would grateful appreciate it if you  check and let me know.

    i hope for your answer.

    UniOTech Corp. (Unique Optical Technology)
    Address : B313, 17, Techno 4-ro, Yuseong-gu, Daejeon, Republic of Korea, postal code 34013
    Tel : +82-42-933-9870~1 / Fax : +82-303-0959-9870 / Mobile : +82-10-5045-9495
    Ji-nam Park/ Assistant manager / Website : http://www.uniotech.kr / E-mail : jinam@uniotech.kr
    LASER, VCSEL, DETECTOR, LASER DRIVER, SCANNER, LENS & CRYSTAL, DOE & BEAM SHAPER, FIBER OPTIC, 광학설계모듈 제작  양산프로그램 제작

  • Hello Ji-Nam,

    From what is shown here it appears that the optical engine is showing lateral color. This is present in all projection technology but can be made more prominent depending on the wave guide design. The projection lens was likely designed for LEDs and is not for specific laser colors.

    What f-number (f/#) is the optical module running? You should likely keep this above f/5 with the laser implementation.

    There are some points you may try:

    • Defocus lens to increase smoothness and color blending
    • Increase source etendue by adding diffuser
    • Increase f/# to that diffraction decreases MTF

    In general, this issue lies in the customer's optical design. They will need to balance their tradeoffs for MTF, efficiency and coupling.

    Regards,

    Austin

  • Hello Ji-Nam,

    I wanted to follow up with this thread. Please let me know if the issue is resolved or if there is any further assitance we might provide.

    Regards,

    Austin