This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCRC410EVM: Power connection of a previous revision

Part Number: DLPLCRC410EVM

Hi

Our customer have purchased the DLPLCRC410EVM in October 2019 through Digikey. It seems to be a previous revision. Can you help to answer his concern below?

The model I have does not have the same power connector as in the datasheet see picture attached). It seems that Digikey have sold an older version of the card... Would it have any compatibility impact on the software? Would it change the performance of the card? And most importantly, could you please send me the documentation so that I can connect the power properly?

Regards,
Roland

  • Hello Roland,

    If it does not have a barrel style receptacle on the board then it should have a 2x4 Molex receptacle that fits the pigtail that should be in the box with the kit.

    If you do not have that pigtail let us know.  The board schematic will show which pins connect to +5V and which connect to Ground.

    Fizix