This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010EVM-LC: About the stop function by temperature

Part Number: DLP3010EVM-LC

Hi

I am still using the DLP3010EVM-LC.

Is there a safety feature that stops due to temperature?
If it is implemented, at what temperature does it stop?
It did not stop even when it was actually warmed to 100 ° C.

Regards,

Tak