This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC410: DLPCRC410EVM

Part Number: DLPC410

Hi team,

We have a customer inquiring about DLPCRC410EVM,Below is the verbatim of his inquiry.

"I want to use dlpcrc410evm (https://www.ti.com/tool/DLPLCRC410EVM) to achieve a 22kHz refresh rate, so I started to understand the APPSFPGA source code provided by TI(DLP(R) Discovery 4100 Applications FPGA Pattern Generator Souce Code version 2). I noticed that in the source code there are some codes for simulation purposes, but testbench files are not provided. So I would like to ask if there are Xilinx ISE project folders containing everything both for with and without DDR2 versions? "

Thank you so much.

  • Hello Yanni,

    We regret that only what is provided there is what is available at this time.

    In order to reach the 22 kHz they will need to use the memory or they will need to build a high speed interface in the APPS_FPGA using the EXP connectors or design their own board.

    Fizix