This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Binary frame rate

Hello there. I am interested in the LC for my project, but I have some questions about it. What is the fastest rate at which we can display static binary images, and that we can actually set up from the control SW? Also, same question but with the video streaming input (HDMI-DVI). I understand the .55 chipset is capable of 5K binary fps, can we achieve that rate with LC by any means, even if it implies developing an expansion card and/or our own code that use any DLLs you provide, in other words is there an SDK available? Thanks in advance.