This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3478: Some problems with testing DLPC-API-1.9

Part Number: DLPC3478


1,In Internal Patterns streaming mode,load the pattern data directly to run the patterns display OK ,if  GenerateAndProgramPatternData,the patterns display is not  my selected patterns ;   

/*------------------------------------------------------------------------------
 * Copyright (c) 2019 Texas Instruments Incorporated - http://www.ti.com/
 *------------------------------------------------------------------------------
 *
 *  Redistribution and use in source and binary forms, with or without
 *  modification, are permitted provided that the following conditions
 *  are met:
 *
 *    Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 *    Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the
 *    distribution.
 *
 *    Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
 *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
 *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
 *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
 *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
 *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
 *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
 *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
 *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
 *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
 *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

/**
 * \file
 * \brief  Sample code for generating internal pattern data and communicating
 *         with the DLP2010-LC and DLP3010-LC EVMs.
 */

#include "dlpc_common.h"
#include "dlpc34xx.h"
#include "dlpc347x_internal_patterns.h"
#include "cypress_i2c.h"
#include "math.h"
#include "stdio.h"
#include "stdint.h"
#include "stdbool.h"
#include "string.h"
#include "time.h"
#include <windows.h> 

#define MAX_WIDTH                         DLP3010_WIDTH
#define MAX_HEIGHT                        DLP3010_HEIGHT

#define NUM_PATTERN_SETS                  1
#define NUM_PATTERN_ORDER_TABLE_ENTRIES   1
#define NUM_ONE_BIT_HORIZONTAL_PATTERNS   0
#define NUM_EIGHT_BIT_HORIZONTAL_PATTERNS 1
#define NUM_ONE_BIT_VERTICAL_PATTERNS     0
#define NUM_EIGHT_BIT_VERTICAL_PATTERNS   6
#define TOTAL_HORIZONTAL_PATTERNS         (NUM_ONE_BIT_HORIZONTAL_PATTERNS + NUM_EIGHT_BIT_HORIZONTAL_PATTERNS)
#define TOTAL_VERTICAL_PATTERNS           (NUM_ONE_BIT_VERTICAL_PATTERNS + NUM_EIGHT_BIT_VERTICAL_PATTERNS)

#define FLASH_WRITE_BLOCK_SIZE            1024
#define FLASH_READ_BLOCK_SIZE             256

#define MAX_WRITE_CMD_PAYLOAD             (FLASH_WRITE_BLOCK_SIZE + 8)
#define MAX_READ_CMD_PAYLOAD              (FLASH_READ_BLOCK_SIZE  + 8)

static uint8_t                                   s_HorizontalPatternData[TOTAL_HORIZONTAL_PATTERNS][MAX_HEIGHT];
static uint8_t                                   s_VerticalPatternData[TOTAL_VERTICAL_PATTERNS][MAX_WIDTH];
static DLPC34XX_INT_PAT_PatternData_s            s_Patterns[TOTAL_VERTICAL_PATTERNS];
static DLPC34XX_INT_PAT_PatternSet_s             s_PatternSets[NUM_PATTERN_SETS];
static DLPC34XX_INT_PAT_PatternOrderTableEntry_s s_PatternOrderTable[NUM_PATTERN_ORDER_TABLE_ENTRIES];

static uint8_t                                   s_WriteBuffer[MAX_WRITE_CMD_PAYLOAD];
static uint8_t                                   s_ReadBuffer[MAX_READ_CMD_PAYLOAD];

static bool                                      s_StartProgramming;
static uint8_t                                   s_FlashProgramBuffer[FLASH_WRITE_BLOCK_SIZE];
static uint16_t                                  s_FlashProgramBufferPtr;

static FILE*                                     s_FilePointer;

#pragma pack(push, 1)
typedef struct {
    unsigned short bfType;
    unsigned int bfSize;
    unsigned short bfReserved1;
    unsigned short bfReserved2;
    unsigned int bfOffBits;
}FileHeader;
#pragma pack(pop)

typedef struct {
    unsigned int biSize;
    int    biWidth;
    int    biHeight;
    unsigned short biPlanes;
    unsigned short biBitCount;
    unsigned int biCompression;
    unsigned int biSizeImage;
    int    biXPelsPerMeter;
    int    biYPelsPerMeter;
    unsigned int biClrUsed;
    unsigned int biClrImportant;
}InfoHeader;

/**
 * Implement the I2C write transaction here. The sample code here sends
 * data to the controller via the Cypress USB-Serial adapter.
 */
uint32_t WriteI2C(uint16_t             WriteDataLength,
	uint8_t*                           WriteData,
	DLPC_COMMON_CommandProtocolData_s* ProtocolData)
{
	bool Status = true;
	//printf("Write I2C Starts, length %d!!! \n", WriteDataLength);
	Status = CYPRESS_I2C_WriteI2C(WriteDataLength, WriteData);
	if (Status != true)
	{
		printf("Write I2C Error!!! \n");
		return FAIL;
	}

	return SUCCESS;
}

/**
 * Implement the I2C write/read transaction here. The sample code here
 * receives data from the controller via the Cypress USB-Serial adapter.
 */
uint32_t ReadI2C(uint16_t              WriteDataLength,
	uint8_t*                           WriteData,
	uint16_t                           ReadDataLength,
	uint8_t*                           ReadData,
	DLPC_COMMON_CommandProtocolData_s* ProtocolData)
{
	bool Status = 0;
	//printf("Write/Read I2C Starts, length %d!!! \n", WriteDataLength);
	Status = CYPRESS_I2C_WriteI2C(WriteDataLength, WriteData);
	if (Status != true)
	{
		printf("Write I2C Error!!! \n");
		return FAIL;
	}

	Status = CYPRESS_I2C_ReadI2C(ReadDataLength, ReadData);
	if (Status != true)
	{
		printf("Read I2C Error!!! \n");
		return FAIL;
	}

	return SUCCESS;
}

/**
 * Initialize the command layer by setting up the read/write buffers and 
 * callbacks.
 */
void InitConnectionAndCommandLayer()
{
    DLPC_COMMON_InitCommandLibrary(s_WriteBuffer,
                                   sizeof(s_WriteBuffer),
                                   s_ReadBuffer,
                                   sizeof(s_ReadBuffer),
                                   WriteI2C,
                                   ReadI2C);

    CYPRESS_I2C_ConnectToCyI2C();
}

void WaitForSeconds(uint32_t Seconds)
{
	uint32_t retTime = (uint32_t)(time(0)) + Seconds;	// Get finishing time.
	while (time(0) < retTime);					        // Loop until it arrives.
}

/**
 * A sample function that generates a 1-bit (binary) 1-D pattern
 * The function fills the byte array Data. Each byte in the in array corresponds
 * to a pixel. For a 1-bit pattern the value of each byte should be 1 or 0.
 */
void PopulateOneBitPatternData(uint16_t Length, uint8_t* Data, uint16_t NumBars)
{
    uint16_t PixelPos  = 0;
    uint16_t BarPos    = 0;
    uint16_t BarWidth  = Length / NumBars;
    uint8_t  PixelData = 0;

    for (; PixelPos < Length; PixelPos++)
    {
        Data[PixelPos] = PixelData;

        BarPos++;
        if (BarPos >= BarWidth)
        {
            BarPos = 0;
            PixelData = (PixelData == 0 ? 1 : 0);
        }
    }
}

static void getData(char* name, uint8_t* data)
{
    FILE *fp = fopen(name, "rb");
    unsigned int size, offset;
    long width, height , bitcount;
    if(NULL == fp)
    {
        printf("open bmp file failed!!!\n");
        return;
    }
    fseek(fp, 0, 0);
    FileHeader file;
    fread(&file, sizeof(FileHeader), 1, fp);
    offset = file.bfOffBits;
    size = file.bfSize;
    InfoHeader head;
    fread(&head, sizeof(InfoHeader), 1, fp);
    width = head.biWidth;
    height = head.biHeight;
    bitcount = head.biBitCount;
    if(0 != fseek(fp, offset, SEEK_SET))
        return;
    int xsize = size - offset;
    auto x = fread(data, xsize, 1, fp);
    printf("fread state: %d!!!\n",x);
    fclose(fp);
}

/**
 * A sample function that generates an 8-bit (gray scale) 1-D pattern
 * The function fills the byte array Data. Each byte in the in array corresponds
 * to a pixel. For an 8-bit pattern the value of each byte can be 0 - 255.
 */
void PopulateEightBitPatternData(uint16_t width, uint16_t height, uint8_t* Data, uint16_t NumBars, uint16_t index)
{
    uint16_t PixelPos     = 0;
    uint16_t BarPos       = 0;
    uint16_t BarWidth     = width / (2 * NumBars);
    uint8_t  PixelData    = 0;
    int16_t  PixelDataInc = (int16_t)ceil(255.0 / BarWidth);
    char name[100];
    uint8_t imagedata[MAX_WIDTH * MAX_HEIGHT] = { 0 };
    sprintf(name, "D:/GIT/DLP/builds/dlpctest/dlpc/img/v0%d.bmp", index);
    printf("name=%s\n", name);
    getData(name, imagedata);

    for (; PixelPos < width; ++PixelPos)
    {
        Data[PixelPos] = imagedata[PixelPos * height];
        //BarPos++;
        //if (BarPos >= BarWidth)
        //{
        //    BarPos    = 0;
        //    PixelDataInc = -PixelDataInc;
        //}
        //PixelData = (uint8_t)(PixelData + PixelDataInc);
    }
}

/**
 * Populates an array of DLPC34XX_INT_PAT_PatternSet_s
 */
void PopulatePatternSetData(uint16_t DMDWidth, uint16_t DMDHeight)
{
    uint8_t                        HorzPatternIdx = 0;
    uint8_t                        VertPatternIdx = 0;
    uint8_t                        PatternIdx     = 0;
    uint8_t                        PatternSetIdx  = 0;
    uint8_t                        Index;
    uint16_t                       NumBars;
    DLPC34XX_INT_PAT_PatternSet_s* PatternSet;

    ///* Create a 1-bit (binary) Horizontal Pattern Set */
    //PatternSet = &s_PatternSets[PatternSetIdx++];
    //PatternSet->BitDepth     = DLPC34XX_INT_PAT_BITDEPTH_ONE;
    //PatternSet->Direction    = DLPC34XX_INT_PAT_DIRECTION_HORIZONTAL;
    //PatternSet->PatternCount = NUM_ONE_BIT_HORIZONTAL_PATTERNS;
    //PatternSet->PatternArray = &s_Patterns[PatternIdx];
    //for (Index = 0; Index < NUM_ONE_BIT_HORIZONTAL_PATTERNS; Index++)
    //{
    //    NumBars = 2 * (Index + 1);
    //    PopulateOneBitPatternData(DMDHeight, s_HorizontalPatternData[HorzPatternIdx], NumBars);
    //    s_Patterns[PatternIdx].PixelArray      = s_HorizontalPatternData[HorzPatternIdx];
    //    s_Patterns[PatternIdx].PixelArrayCount = DMDHeight;
    //    PatternIdx++;
    //    HorzPatternIdx++;
    //}
    //
    ///* Create a 1-bit (binary) Vertical Pattern Set */
    //PatternSet = &s_PatternSets[PatternSetIdx++];
    //PatternSet->BitDepth     = DLPC34XX_INT_PAT_BITDEPTH_ONE;
    //PatternSet->Direction    = DLPC34XX_INT_PAT_DIRECTION_VERTICAL;
    //PatternSet->PatternCount = NUM_ONE_BIT_VERTICAL_PATTERNS;
    //PatternSet->PatternArray = &s_Patterns[PatternIdx];
    //for (Index = 0; Index < NUM_ONE_BIT_VERTICAL_PATTERNS; Index++)
    //{
    //    NumBars = 2 * (Index + 1);
    //    PopulateOneBitPatternData(DMDWidth, s_VerticalPatternData[VertPatternIdx], NumBars);
    //    s_Patterns[PatternIdx].PixelArray      = s_VerticalPatternData[VertPatternIdx];
    //    s_Patterns[PatternIdx].PixelArrayCount = DMDWidth;
    //    PatternIdx++;
    //    VertPatternIdx++;
    //}

    ///* Create an 8-bit (grayscale) Horizontal Pattern Set */
    //PatternSet = &s_PatternSets[PatternSetIdx++];
    //PatternSet->BitDepth     = DLPC34XX_INT_PAT_BITDEPTH_EIGHT;
    //PatternSet->Direction    = DLPC34XX_INT_PAT_DIRECTION_HORIZONTAL;
    //PatternSet->PatternCount = NUM_EIGHT_BIT_HORIZONTAL_PATTERNS;
    //PatternSet->PatternArray = &s_Patterns[PatternIdx];
    //for (Index = 0; Index < NUM_EIGHT_BIT_HORIZONTAL_PATTERNS; Index++)
    //{
    //    NumBars = 2 * (Index + 1);
    //    PopulateEightBitPatternData(DMDHeight, s_HorizontalPatternData[HorzPatternIdx], NumBars);
    //    s_Patterns[PatternIdx].PixelArray      = s_HorizontalPatternData[HorzPatternIdx];
    //    s_Patterns[PatternIdx].PixelArrayCount = DMDHeight;
    //    PatternIdx++;
    //    HorzPatternIdx++;
    //}

    /* Create an 8-bit (grayscale) Vertical Pattern Set */
    PatternSet = &s_PatternSets[PatternSetIdx++];
    PatternSet->BitDepth     = DLPC34XX_INT_PAT_BITDEPTH_EIGHT;
    PatternSet->Direction    = DLPC34XX_INT_PAT_DIRECTION_VERTICAL;
    PatternSet->PatternCount = NUM_EIGHT_BIT_VERTICAL_PATTERNS;
    PatternSet->PatternArray = &s_Patterns[PatternIdx];
    for (Index = 0; Index < NUM_EIGHT_BIT_VERTICAL_PATTERNS; Index++)
    {
        NumBars = 2 * (Index + 1);
        PopulateEightBitPatternData(DMDWidth, DMDHeight, s_VerticalPatternData[VertPatternIdx], NumBars, PatternIdx);
        s_Patterns[PatternIdx].PixelArray      = s_VerticalPatternData[VertPatternIdx];
        s_Patterns[PatternIdx].PixelArrayCount = DMDWidth;
        PatternIdx++;
        VertPatternIdx++;
    }
}

/**
 * Populates an array of DLPC34XX_INT_PAT_PatternOrderTableEntry_s
 */
void PopulatePatternTableData()
{
    DLPC34XX_INT_PAT_PatternOrderTableEntry_s* PatternOrderTableEntry;
    uint32_t                                   PatternOrderTableIdx = 0;
    uint32_t                                   PatternSetIdx        = 0;

    /* Pattern Table Entry 0 - uses Pattern Set 0 */
    PatternOrderTableEntry = &s_PatternOrderTable[PatternOrderTableIdx++];
    PatternOrderTableEntry->PatternSetIndex                        = PatternSetIdx;
    PatternOrderTableEntry->NumDisplayPatterns                     = s_PatternSets[PatternSetIdx++].PatternCount;
    PatternOrderTableEntry->IlluminationSelect                     = DLPC34XX_INT_PAT_ILLUMINATION_BLUE;
    PatternOrderTableEntry->InvertPatterns                         = false;
    PatternOrderTableEntry->IlluminationTimeInMicroseconds         = 9400;
    PatternOrderTableEntry->PreIlluminationDarkTimeInMicroseconds  = 500;
    PatternOrderTableEntry->PostIlluminationDarkTimeInMicroseconds = 100;

    ///* Pattern Table Entry 1 - uses Pattern Set 1 */
    //PatternOrderTableEntry = &s_PatternOrderTable[PatternOrderTableIdx++];
    //PatternOrderTableEntry->PatternSetIndex                        = PatternSetIdx;
    //PatternOrderTableEntry->NumDisplayPatterns                     = s_PatternSets[PatternSetIdx++].PatternCount;
    //PatternOrderTableEntry->IlluminationSelect                     = DLPC34XX_INT_PAT_ILLUMINATION_GREEN;
    //PatternOrderTableEntry->InvertPatterns                         = false;
    //PatternOrderTableEntry->IlluminationTimeInMicroseconds         = 5000;
    //PatternOrderTableEntry->PreIlluminationDarkTimeInMicroseconds  = 250;
    //PatternOrderTableEntry->PostIlluminationDarkTimeInMicroseconds = 1000;

    ///* Pattern Table Entry 2 - uses Pattern Set 2 */
    //PatternOrderTableEntry = &s_PatternOrderTable[PatternOrderTableIdx++];
    //PatternOrderTableEntry->PatternSetIndex                        = PatternSetIdx;
    //PatternOrderTableEntry->NumDisplayPatterns                     = s_PatternSets[PatternSetIdx++].PatternCount;
    //PatternOrderTableEntry->IlluminationSelect                     = DLPC34XX_INT_PAT_ILLUMINATION_BLUE;
    //PatternOrderTableEntry->InvertPatterns                         = false;
    //PatternOrderTableEntry->IlluminationTimeInMicroseconds         = 5000;
    //PatternOrderTableEntry->PreIlluminationDarkTimeInMicroseconds  = 250;
    //PatternOrderTableEntry->PostIlluminationDarkTimeInMicroseconds = 1000;

    ///* Pattern Table Entry 3 - uses Pattern Set 3 */
    //PatternOrderTableEntry = &s_PatternOrderTable[PatternOrderTableIdx++];
    //PatternOrderTableEntry->PatternSetIndex                        = PatternSetIdx;
    //PatternOrderTableEntry->NumDisplayPatterns                     = s_PatternSets[PatternSetIdx++].PatternCount;
    //PatternOrderTableEntry->IlluminationSelect                     = DLPC34XX_INT_PAT_ILLUMINATION_RGB;
    //PatternOrderTableEntry->InvertPatterns                         = false;
    //PatternOrderTableEntry->IlluminationTimeInMicroseconds         = 11000;
    //PatternOrderTableEntry->PreIlluminationDarkTimeInMicroseconds  = 250;
    //PatternOrderTableEntry->PostIlluminationDarkTimeInMicroseconds = 1000;
}

void CopyDataToFlashProgramBuffer(uint8_t* Length, uint8_t** DataPtr)
{
    while ((*Length >= 1) &&
           (s_FlashProgramBufferPtr < sizeof(s_FlashProgramBuffer)))
    {
        s_FlashProgramBuffer[s_FlashProgramBufferPtr] = **DataPtr;
        s_FlashProgramBufferPtr++;
        (*DataPtr)++;
        (*Length)--;
    }
}

void ProgramFlashWithDataInBuffer(uint16_t Length)
{
    s_FlashProgramBufferPtr = 0;

    if (s_StartProgramming)
    {
        s_StartProgramming = false;
        DLPC34XX_WriteFlashStart(Length, s_FlashProgramBuffer);
    }
    else
    {
        DLPC34XX_WriteFlashContinue(Length, s_FlashProgramBuffer);
    }
}

void WriteDataToFile(uint8_t Length, uint8_t* Data)
{
    fwrite(Data, 1, Length, s_FilePointer);
}

void GenerateAndWritePatternDataToFile(DLPC34XX_INT_PAT_DMD_e DMD, char* FilePath, bool EastWestFlip)
{
    s_FilePointer = fopen(FilePath, "wb");

    /* Generate pattern data and write it to the flash.
     * The DLPC34XX_INT_PAT_GeneratePatternDataBlock() function will call the
     * WriteDataToFile() function several times while it packs sections of the
     * pattern data.
     */
    DLPC34XX_INT_PAT_GeneratePatternDataBlock(DMD,
                                              NUM_PATTERN_SETS,
                                              s_PatternSets,
                                              NUM_PATTERN_ORDER_TABLE_ENTRIES,
                                              s_PatternOrderTable,
                                              WriteDataToFile,
											  EastWestFlip);

    fclose(s_FilePointer);
}

void BufferPatternDataAndProgramToFlash(uint8_t Length, uint8_t* Data)
{
    /* Copy data that can fit in the flash programming buffer */
    CopyDataToFlashProgramBuffer(&Length, &Data);

    /* Write data to flash if the buffer is full */
    if (s_FlashProgramBufferPtr >= sizeof(s_FlashProgramBuffer))
    {
        ProgramFlashWithDataInBuffer((uint16_t)sizeof(s_FlashProgramBuffer));
    }

    /* Copy remaining data (if any) to the flash programming buffer */
    CopyDataToFlashProgramBuffer(&Length, &Data);
}

void GenerateAndProgramPatternData(DLPC34XX_INT_PAT_DMD_e DMD, bool EastWestFlip)
{
    s_StartProgramming = true;
    s_FlashProgramBufferPtr = 0;

    /* Let the controller know that we're going to program pattern data */
    DLPC34XX_WriteFlashDataTypeSelect(DLPC34XX_FDTS_ENTIRE_SENS_PATTERN_DATA);
    
    /* Erase the flash sectors that store pattern data */
    DLPC34XX_WriteFlashErase();
    Sleep(2000);
	/* Read Short Status to make sure Erase is completed */
	DLPC34XX_ShortStatus_s ShortStatus;
	do
	{
		DLPC34XX_ReadShortStatus(&ShortStatus);
	} while (ShortStatus.FlashEraseComplete == DLPC34XX_FE_NOT_COMPLETE);

	/* To program the flash, send blocks of data of up to 1024 bytes
     * to the controller at a time. Repeat the process until the entire
     * data is programmed to the flash.
     * Let the controller know the size of a data block that will be 
     * transferred at a time.
     */
    DLPC34XX_WriteFlashDataLength(sizeof(s_FlashProgramBuffer));

    /* Generate pattern data and program it to the flash.
     * 
     * The DLPC34XX_INT_PAT_GeneratePatternDataBlock() function calls the
     * BufferPatternDataAndProgramToFlash() function several times while it
     * generates pattern data.
     * 
     * The BufferPatternDataAndProgramToFlash() function buffers data received,
     * programming the buffer content only when it is full. This is done in an
     * effort to make flash writes more efficient, overall greatly reducing the
     * time it takes to program the pattern data.
     * 
     * After returning from the DLPC34XX_INT_PAT_GeneratePatternBlock() function,
     * check if there is any data left in the buffer and program it. This needs 
     * to be done since the BufferPatternDataAndProgramToFlash() function only 
     * programs the buffer content if full.
     */
    DLPC34XX_INT_PAT_GeneratePatternDataBlock(DMD,
                                              NUM_PATTERN_SETS,
                                              s_PatternSets,
                                              NUM_PATTERN_ORDER_TABLE_ENTRIES,
                                              s_PatternOrderTable,
                                              BufferPatternDataAndProgramToFlash,
											  EastWestFlip);
    if (s_FlashProgramBufferPtr > 0)
    {
        /* Resend the block size since it could be less than 
         * the previously specified size
         */
        DLPC34XX_WriteFlashDataLength(s_FlashProgramBufferPtr);

        ProgramFlashWithDataInBuffer(s_FlashProgramBufferPtr);
    }
}

void LoadPatternOrderTableEntryfromFlash()
{
	DLPC34XX_PatternOrderTableEntry_s PatternOrderTableEntry;

    PatternOrderTableEntry.PatSetIndex = 0;
    PatternOrderTableEntry.NumberOfPatternsToDisplay = 6;
    PatternOrderTableEntry.RedIlluminator = DLPC34XX_IE_DISABLE;
    PatternOrderTableEntry.GreenIlluminator = DLPC34XX_IE_DISABLE;
    PatternOrderTableEntry.BlueIlluminator = DLPC34XX_IE_ENABLE;
    PatternOrderTableEntry.PatternInvertLsword = 0;
    PatternOrderTableEntry.PatternInvertMsword = 0;
    PatternOrderTableEntry.IlluminationTime = 9400;
    PatternOrderTableEntry.PreIlluminationDarkTime = 500;
    PatternOrderTableEntry.PostIlluminationDarkTime = 100;

	/* Reload from Flash */
	DLPC34XX_WritePatternOrderTableEntry(DLPC34XX_WC_RELOAD_FROM_FLASH, &PatternOrderTableEntry);
}

void LoadPatternOrderTableEntry(uint8_t PatternSetIndex)
{
	DLPC34XX_PatternOrderTableEntry_s PatternOrderTableEntry;

	/* Set PatternOrderTableEntry to select specific Pattern Set and configure settings */
	PatternOrderTableEntry.PatSetIndex = 0;
	PatternOrderTableEntry.NumberOfPatternsToDisplay = PatternSetIndex;
	PatternOrderTableEntry.RedIlluminator = DLPC34XX_IE_DISABLE;
	PatternOrderTableEntry.GreenIlluminator = DLPC34XX_IE_DISABLE;
	PatternOrderTableEntry.BlueIlluminator = DLPC34XX_IE_ENABLE;
	PatternOrderTableEntry.PatternInvertLsword = 0;
	PatternOrderTableEntry.PatternInvertMsword = 0;
	PatternOrderTableEntry.IlluminationTime = 9400;
	PatternOrderTableEntry.PreIlluminationDarkTime = 500;
	PatternOrderTableEntry.PostIlluminationDarkTime = 100;
	DLPC34XX_WritePatternOrderTableEntry(DLPC34XX_WC_START, &PatternOrderTableEntry);
}

void WriteTestPatternGridLines()
{
	/* Write Input Image Size */
	DLPC34XX_WriteInputImageSize(MAX_WIDTH, MAX_HEIGHT);

	/* Write Image Crop */
	DLPC34XX_WriteImageCrop(0, 0, MAX_WIDTH, MAX_HEIGHT);

	/* Write Display Size */
	DLPC34XX_WriteDisplaySize(0, 0, MAX_WIDTH, MAX_HEIGHT);

	/* Write Grid Lines */
	DLPC34XX_GridLines_s GridLines;
	GridLines.Border = DLPC34XX_BE_ENABLE;
	GridLines.BackgroundColor = DLPC34XX_C_GREEN;
	GridLines.ForegroundColor = DLPC34XX_C_MAGENTA;
	GridLines.HorizontalForegroundLineWidth = 0xF;
	GridLines.HorizontalBackgroundLineWidth = 0xF;
	GridLines.VerticalForegroundLineWidth = 0xF;
	GridLines.VerticalBackgroundLineWidth = 0xF;
	DLPC34XX_WriteGridLines(&GridLines);

	DLPC34XX_WriteOperatingModeSelect(DLPC34XX_OM_TEST_PATTERN_GENERATOR);
	WaitForSeconds(5);
}

void WriteTestPatternColorBar()
{
	/* Write Input Image Size */
	DLPC34XX_WriteInputImageSize(MAX_WIDTH, MAX_HEIGHT);

	/* Write Image Crop */
	DLPC34XX_WriteImageCrop(0, 0, MAX_WIDTH, MAX_HEIGHT);

	/* Write Display Size */
	DLPC34XX_WriteDisplaySize(0, 0, MAX_WIDTH, MAX_HEIGHT);

	/* Write Color Bar & Select Test Pattern */
	DLPC34XX_WriteColorbars(DLPC34XX_BE_ENABLE);

	DLPC34XX_WriteOperatingModeSelect(DLPC34XX_OM_TEST_PATTERN_GENERATOR);
	WaitForSeconds(5);
}

void WriteLookSelect(uint8_t LookNumber)
{
	/* Read Current Operating Mode Selected */
	DLPC34XX_OperatingMode_e OperatingMode;
	DLPC34XX_ReadOperatingModeSelect(&OperatingMode);

	/* Write RGB LED Current (based on Flash data) */
	DLPC34XX_WriteRgbLedCurrent(0x03E8, 0x03E8, 0x03E8);

	/* Select Look */
	DLPC34XX_WriteLookSelect(LookNumber);
	WaitForSeconds(2);

	/* Submit Write Splash Screen Execute if in Splash Mode */
	if ((OperatingMode == DLPC34XX_OM_SPLASH_SCREEN ) ||
		(OperatingMode == DLPC34XX_OM_SENS_SPLASH_PATTERN))
	{
		DLPC34XX_WriteSplashScreenExecute();
		WaitForSeconds(2);
	}
	WaitForSeconds(5);
}

void LoadPreBuildPatternData()
{
	/* write up to 1024 bytes of data */
	uint8_t PatternDataArray[1024];

	/* Pattern File assumes to be in the \build\vs2017\dlpc347x folder */
	s_FilePointer = fopen("1.bin", "rb");
	if (!s_FilePointer)
	{
		printf("Error opening the binary file!");
		return;
	}
	fseek(s_FilePointer, 0, SEEK_END);
	uint32_t PatternDataSize = ftell(s_FilePointer);
	fseek(s_FilePointer, 0, SEEK_SET);

	/* Select Flash Data Block and Erase the Block */
	DLPC34XX_WriteFlashDataTypeSelect(DLPC34XX_FDTS_ENTIRE_SENS_PATTERN_DATA);
	DLPC34XX_WriteFlashErase();

	/* Read Short Status to make sure Erase is completed */
	DLPC34XX_ShortStatus_s ShortStatus;
	do
	{
		DLPC34XX_ReadShortStatus(&ShortStatus);
	} while (ShortStatus.FlashEraseComplete == DLPC34XX_FE_NOT_COMPLETE);

	DLPC34XX_WriteFlashDataLength(1024);
	fread(PatternDataArray, sizeof(PatternDataArray), 1, s_FilePointer);
	DLPC34XX_WriteFlashStart(1024, PatternDataArray);

	int32_t BytesLeft = PatternDataSize - 1024;
	do
	{
		fread(PatternDataArray, sizeof(PatternDataArray), 1, s_FilePointer);
		DLPC34XX_WriteFlashContinue(1024, PatternDataArray);

		BytesLeft = BytesLeft - 1024;
	} while (BytesLeft > 0);

	fclose(s_FilePointer);
}


void WriteLabbCaic()
{
	//SetIntelliBright(bool EnableLabb, uint8_t LabbStrength, uint8_t LabbSharpness,
	//                 bool EnableCaic, double CaicGain, bool EnableCaicDisplay,
	//                 double *MaxPower, uint16_t *CaicRed, uint16_t *CaicGreen, uint16_t *CaicBlue)

	DLPC34XX_WriteLocalAreaBrightnessBoostControl(DLPC34XX_LC_MANUAL, 5, 60);		/* Enable LABB */
	DLPC34XX_WriteCaicImageProcessingControl(DLPC34XX_CGDS_P1024, true, 2.5, 0);	/* Enable CAIC */

	DLPC34XX_WriteLedOutputControlMethod(DLPC34XX_LCM_AUTOMATIC);

	double MaxPower;
	DLPC34XX_ReadCaicLedMaxAvailablePower(&MaxPower);

	uint16_t CaicRedCurrent, CaicGreenCurrent, CaicBlueCurrent;
	DLPC34XX_ReadCaicRgbLedCurrent(&CaicRedCurrent, &CaicGreenCurrent, &CaicBlueCurrent);

	DLPC34XX_OperatingMode_e CurrentOperatingMode;
	DLPC34XX_ReadOperatingModeSelect(&CurrentOperatingMode);

	if ((CurrentOperatingMode == DLPC34XX_OM_SPLASH_SCREEN) ||
		(CurrentOperatingMode == DLPC34XX_OM_SENS_SPLASH_PATTERN))
	{
		DLPC34XX_WriteSplashScreenExecute();
		WaitForSeconds(2);
	}
	WaitForSeconds(5);
}

void LoadFirmware()
{
	/* write up to 1024 bytes of data */
	uint8_t FlashDataArray[1024];

	/* Pattern File assumes to be in the \build\vs2017\dlpc343x folder */
	s_FilePointer = fopen("dlpc3478_7.3.1.img", "rb");
	if (!s_FilePointer)
	{
		printf("Error opening the flash image file!");
		return;
	}
	fseek(s_FilePointer, 0, SEEK_END);
	uint32_t FlashDataSize = ftell(s_FilePointer);
	fseek(s_FilePointer, 0, SEEK_SET);

	/* Select Flash Data Block and Erase the Block */
	DLPC34XX_WriteFlashDataTypeSelect(DLPC34XX_FDTS_ENTIRE_FLASH);
	DLPC34XX_WriteFlashErase();

	/* Read Short Status to make sure Erase is completed */
	DLPC34XX_ShortStatus_s ShortStatus;
	do
	{
		WaitForSeconds(1);
		DLPC34XX_ReadShortStatus(&ShortStatus);
	} while (ShortStatus.FlashEraseComplete == DLPC34XX_FE_NOT_COMPLETE);

	DLPC34XX_WriteFlashDataLength(1024);
	fread(FlashDataArray, sizeof(FlashDataArray), 1, s_FilePointer);
	DLPC34XX_WriteFlashStart(1024, FlashDataArray);

	int32_t BytesLeft = FlashDataSize - 1024;
	do
	{
		fread(FlashDataArray, sizeof(FlashDataArray), 1, s_FilePointer);
		DLPC34XX_WriteFlashContinue(1024, FlashDataArray);

		BytesLeft = BytesLeft - 1024;
	} while (BytesLeft > 0);

	fclose(s_FilePointer);
    printf("LoadFirmware successful!");
}

void main()
{
    InitConnectionAndCommandLayer();
    /* TI DLP Pico EVMs use a GPIO handshake scheme for the controller I2C bus
     * arbitration. Call this method if using a TI EVM, remove otherwise
     */
	bool Status = CYPRESS_I2C_RequestI2CBusAccess();
	if (Status != true)
	{
		printf("Error Request I2C Bus ACCESS!!!");
		return;
	}
	DLPC34XX_ControllerDeviceId_e DeviceId = 0;
	DLPC34XX_ReadControllerDeviceId(&DeviceId);
	printf("Controller Devicde Id = %d \n", DeviceId);

	uint16_t PixelsPerLine, LinesPerFrame;
	DLPC34XX_ReadInputImageSize(&PixelsPerLine, &LinesPerFrame);
	printf("Input Image Size = 0x%x, 0x%x \n", PixelsPerLine, LinesPerFrame);

	/* ***** Write Test Patterns ***** */
	/*WriteTestPatternGridLines();
	WriteTestPatternColorBar();

	WriteLabbCaic();*/

	/* ***** Test Internal Pattern Sensing ***** */
	bool LoadFromFirmware = false;
	bool LoadFromFile = false;	// Switch to load pattern from saved file or generated

	if (LoadFromFirmware)
	{
		LoadFirmware();
	}
	else if (LoadFromFile)
	{
		/* Load pre-build Pattern Table and Sets */
		LoadPreBuildPatternData();
		LoadPatternOrderTableEntryfromFlash();
	}
	else
	{
		/* Prepare the data for pattern data block generation */
		PopulatePatternSetData(MAX_WIDTH, MAX_HEIGHT);
		PopulatePatternTableData();

		/* Stop pattern display */
		DLPC34XX_WriteInternalPatternControl(DLPC34XX_PC_STOP, 0);

		/* Generate and program the pattern data to the controller flash */
		GenerateAndProgramPatternData(DLPC34XX_INT_PAT_DMD_DLP3010, false);

		/* Load Pattern Order Table Entry from Flash */
		LoadPatternOrderTableEntryfromFlash();

		/* Generate and write pattern data to a file */
		GenerateAndWritePatternDataToFile(DLPC34XX_INT_PAT_DMD_DLP3010, "pattern_data.bin", false);
	}

    /* Display patterns */
    DLPC34XX_WriteOperatingModeSelect(DLPC34XX_OM_SENS_INTERNAL_PATTERN);
    DLPC34XX_WriteInternalPatternControl(DLPC34XX_PC_START, 0xFF);

	WaitForSeconds(10);
	DLPC34XX_WriteInternalPatternControl(DLPC34XX_PC_STOP, 0);

	CYPRESS_I2C_RelinquishI2CBusAccess();
}
img.rar

Is there a problem with the code?

2,The same hardware, I use the GUI to control it repeatedly is ok,but the Demo will  offen display"Write/read I2C Error!!!"(CY_ERROR_I2C_DEVICE_BUSY,   CY_ERROR_I2C_NAK_ERRORCY_ERROR_IO_TIMEOUT),then I should update Firmware,what happened?thanks!

  • User,

    Are you accessing the flash memory in your script? If the system is working OK within the GUI, but not within your script, you could be encountering an issue because you are writing I2C commands too quickly. For example, sending I2C commands while the DLPC is attempting to access the EEPROM flash memory may cause the system to hang.

    Do you know which commands are triggering the R/W error? I recommend you try adjusting these commands or adding write delays to see if that alleviates the issue.

    Best Regards,

    Philippe Dollo

  • Hi Philippe,

          1,After I added a delay in this position, ”Write I2C Error!!!“ appearance has decreased significantly ,but it still happens occasionally, Increase the waiting time has no effect,what should I do?

           

       2,As shown below,"read I2C Error!!!" appears in this position,but I can't add delay,do you have any suggestion?

         

    3, when choosed GenerateAndProgramPatternData Process,the patterns display is not  my selected patterns ?

     Thanks,

  • User,

    Two suggestions from me:

    1. One approach you could take here is to attach a probe to the EEPROM Flash Device SPI Bus to monitor for activity. That way, you can see what commands are trying to perform a memory read from EEPROM and for how long. This would give you an indication as to whether there are any memory accesses you are not considering in your script.

    2. You may also want to try using the status register and short status register commands (0xD0 and 0xD1 in the programmer's guide https://www.ti.com/lit/ug/dlpu075a/dlpu075a.pdf) to see if you can monitor for I2C errors. 

    The above should help you build a profile of your system's activity during the failure conditions. That way, you can add only enough delay as is necessary to ensure your system is functioning. You may also find if there are particular commands that are giving you a lot of trouble.

    Best Regards,

    Philippe Dollo