This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have the WD-73737 DLP TV from Mitsubishi. I noticed a lighter, halo effect, on the lower portion of the screen a few years back and remained but did not get worse till now. About 1.5 yrs ago, starting noticing a white dot, and today had around 8 noticeable, but when close to screen can see black dots as well. Went ahead and replaced the chip and both white dots and haze are fixed.
I understand the white dots are the mirrors getting stuck. However, the white haze is not well documented online. It appears to me to be on the inside of the glass above the mirrors. See 2 pics below, the first shows haze on top and shows it’s on glass and not mirror.
This second pic is from directly above. I actually see haze on top and bottom of the glass, however on the bottom, it is below the mirrors and therefore not noticeable on the TV.
Found another similar pic with haze in online forum
Hi,
Haze can be caused when the DMD package seal is broken and moisture gets into the DMD chip. Over time, the moisture can permeate around the DMD.
Frank Xu