This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NULL_LINK_COPY_TYPE_BITSTREAM_FILE mode for file write

Hello friends,

     I want to record video data on to an external hard disk.

My use case has the following structure:

 Capture -> Dup -> Display_Video

Dup ->Null

GrpxSrc -> Display_Grpx

I want to write to a file using Null Link.

 

I am setting the null link parameter as follows in my chain:

 

pPrm->dumpDataType = NULL_LINK_COPY_TYPE_BITSTREAM_FILE;

 

I have assigned the dumpdatatype, but I found that  the "NULL_LINK_COPY_TYPE_BITSTREAM_FILE" mode has not been implemented in nullLink_tsk.c in links_fw/src/rtos/links_common/

 

Should I use the "NULL_LINK_COPY_TYPE_BITSTREAM_FILE" implementation under  links_fw/src/hlos/links_a15/ ?

 

Please give your views and suggestions in this regard.

Best Regards,

Vijay

  • Hello Vijay,

    You can use NULL_LINK_COPY_TYPE_FILE with data type as SYSTEM_BUFFER_TYPE_BITSTREAM.

    I am assuming here you are capturing the bitstream data here and not YUV. Also wondering how you would be displaying the bitstream data as i dont see any link in between capture and display

  • Hello Prasad,
    I am using the SDK D3_VISION_SDK_03_02_63_00_RC_TDA2X_RVP_LINUX.I could not find the NULL_LINK_COPY_TYPE_FILE mode in my SDK.Could you please let me know the right mode for this SDK? On second thoughts I feel YUV data can also be used.So please suggest the mode and data type for YUV data in the SDK mentioned above.

    Best Regards,
    Vijay
  • Hello Vijay,

    What is data format for you YUV steam? Is it 420 or 422? 

  • Hello Prasad,
    The data format is 420.

    Best Regards,
    Vijay
  • Vijay,

    NULL_LINK_COPY_TYPE_FILE is supported in the NULL link. You can check link source file for more details. (vision_sdk\links_fw\src\hlos\links_a15\null\nullLink_tsk.c)

    Set your null link to run on A15 by Dup ->Null (A15) and edit use-case main file to add NULL link configuration.

    You can refer to X:\vsdk_latest\vision_sdk\apps\src\hlos\adas\src\usecases\null_src_decode_display\ for configuration details (this use-case uses NULL source)
  • Hello Prasad,
    Thank you for the answer.But unfortunately I did not have NULL_LINK_COPY_TYPE_FILE in my nullLink_tsk.c under hlos.Perhaps my SDK doesn't have it.In the meanwhile I used NULL_LINK_COPY_TYPE_BITSTREAM_FILE and saved the stream in a .mpeg file.I found the size was very small for a 2 minute video from a camera having a resolution of 1280x1080(OV10640).It was only 99 KB.I was not sure how to open this file.Are there decoders to decode this file.I understand that the compression ratio is very high.Please let me know how to reconstruct the video from this file.Also please let me know if .mpeg or .h264 is the correct format to save a bitstream file.If possible please give me the nullLink_tsk.c file which has NULL_LINK_COPY_TYPE_FILE in it.I will use that file and build my usecase.

    Thanking you in advance,

    Best Regards,
    Vijay
  • Vijay,

    What is SDK version your are using? NULL_LINK_COPY_TYPE_FILE is supported in almost all releases.
    Using bitstream option is not correct as it is for encoded data and what you have here is raw data.
    Can you please share your nulllink_task.c?

    how to open this file.Are there decoders to decode this file.
    >> You can use ffplay to play these files
    Also please let me know if .mpeg or .h264 is the correct format to save a bitstream file
    >> extension should be depending on how you are encoding data in the VSDK use-case. But anyway it should not matter as ffplay would read it from metadata and not from extension
  • Hello Prasad,

     Please find my nullLink_tsk.c attached.

    I am using the following SDK:

    D3_VISION_SDK_03_02_63_00_RC_TDA2X_RVP_LINUX

    Best Regards,

    Vijay

    /*
    Copyright (c) [2012 - 2017] Texas Instruments Incorporated
    
    All rights reserved not granted herein.
    
    Limited License.
    
     Texas Instruments Incorporated grants a world-wide, royalty-free, non-exclusive
     license under copyrights and patents it now or hereafter owns or controls to
     make,  have made, use, import, offer to sell and sell ("Utilize") this software
     subject to the terms herein.  With respect to the foregoing patent license,
     such license is granted  solely to the extent that any such patent is necessary
     to Utilize the software alone.  The patent license shall not apply to any
     combinations which include this software, other than combinations with devices
     manufactured by or for TI ("TI Devices").  No hardware patent is licensed
     hereunder.
    
     Redistributions must preserve existing copyright notices and reproduce this
     license (including the above copyright notice and the disclaimer and
     (if applicable) source code license limitations below) in the documentation
     and/or other materials provided with the distribution
    
     Redistribution and use in binary form, without modification, are permitted
     provided that the following conditions are met:
    
     * No reverse engineering, decompilation, or disassembly of this software
       is permitted with respect to any software provided in binary form.
    
     * Any redistribution and use are licensed by TI for use only with TI Devices.
    
     * Nothing shall obligate TI to provide you with source code for the software
       licensed and provided to you in object code.
    
     If software source code is provided to you, modification and redistribution of
     the source code are permitted provided that the following conditions are met:
    
     * Any redistribution and use of the source code, including any resulting
       derivative works, are licensed by TI for use only with TI Devices.
    
     * Any redistribution and use of any object code compiled from the source code
       and any resulting derivative works, are licensed by TI for use only with TI
       Devices.
    
     Neither the name of Texas Instruments Incorporated nor the names of its
     suppliers may be used to endorse or promote products derived from this software
     without specific prior written permission.
    
     DISCLAIMER.
    
     THIS SOFTWARE IS PROVIDED BY TI AND TI�S LICENSORS "AS IS" AND ANY EXPRESS OR
     IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF
     MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
     IN NO EVENT SHALL TI AND TI�S LICENSORS BE LIABLE FOR ANY DIRECT, INDIRECT,
     INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
     LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR
     PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF
     LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE
     OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF
     ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    */
    
    /**
      ******************************************************************************
     * \file nullLink_tsk.c
     *
     * \brief  This file has the implementation of DUP Link API
     **
     *           This file implements the state machine logic for this link.
     *           A message command will cause the state machine
     *           to take some action and then move to a different state.
     *
     * \version 0.0 (Jun 2014) : [YM] First version ported to Linux
     *
     *******************************************************************************
     */
    
    /*******************************************************************************
     *  INCLUDE FILES
     *******************************************************************************
     */
    #include "nullLink_priv.h"
    
    /**
     *******************************************************************************
     * \brief Link object, stores all link related information
     *******************************************************************************
     */
    NullLink_Obj gNullLink_obj[NULL_LINK_OBJ_MAX];
    
    /**
     *******************************************************************************
     * \brief Null Link can be used to take input from a link and then without doing
     *   anything return it back to the same link. This useful when a link output
     *   cannot be given to any other link for testing purpose we just want to run
     *   a given link but not really use the output. In such cases the output queue
     *   of link can be connected to a Null link. The null link will operate like
     *   any other link from interface point of view. But it wont do anything with
     *   the frames it gets. It will simply return it back to the sending link. This
     *   function simply does the following
     *
     *     - Copies the user passed create params into the link object create params
     *     - resets received frame count to zero
     *
     * \param  pObj     [IN]  Null link instance handle
     * \param  pPrm     [IN]  Create params for Null link
     *
     * \return status   SYSTEM_LINK_STATUS_SOK on success
     *
     *******************************************************************************
    */
    Int32 NullLink_drvCreate(NullLink_Obj * pObj, NullLink_CreateParams * pPrm)
    {
        Int32 status;
        UInt16 inQue;
        System_LinkInfo inTskInfo;
    
        Vps_printf(" NULL Link: Create in progress !!!\n");
    
        memcpy(&pObj->createArgs, pPrm, sizeof(pObj->createArgs));
        OSA_assert(pObj->createArgs.numInQue < NULL_LINK_MAX_IN_QUE);
    
        pObj->recvCount= 0;
    
        for (inQue = 0; inQue < pPrm->numInQue; inQue++)
        {
            status =
                System_linkGetInfo(pPrm->inQueParams[inQue].prevLinkId,
                                   &inTskInfo);
            OSA_assert(status == SYSTEM_LINK_STATUS_SOK);
            OSA_assert(pPrm->inQueParams[inQue].prevLinkQueId <
                         inTskInfo.numQue);
    
            pObj->inQueInfo[inQue]
                =
                    inTskInfo.queInfo
                [pPrm->inQueParams[inQue].prevLinkQueId];
        }
    
        Vps_printf(" NULL Link: Create done !!!\n");
    
        return SYSTEM_LINK_STATUS_SOK;
    }
    
    /**
     *******************************************************************************
     * \brief Null Link just receives incoming buffers and returns back to the
     *   sending link. This function does the same
     *
     * \param  pObj     [IN]  Null link instance handle
     *
     * \return status   SYSTEM_LINK_STATUS_SOK on success
     *
     *******************************************************************************
    */
    Int32 NullLink_drvProcessFrames(NullLink_Obj * pObj)
    {
        System_LinkInQueParams *pInQueParams;
        System_BufferList bufList;
        UInt32 queId, bufId, chNum;
        System_LinkChInfo *pChInfo;
    
        for (queId = 0; queId < pObj->createArgs.numInQue; queId++)
        {
            pInQueParams = &pObj->createArgs.inQueParams[queId];
    
            System_getLinksFullBuffers(pInQueParams->prevLinkId,
                                      pInQueParams->prevLinkQueId, &bufList);
    
            if (bufList.numBuf)
            {
                System_BitstreamBuffer *bitstreamBuf;
                pObj->recvCount += bufList.numBuf;
                /* File Write enabled for channels only from first inputQ (Q0) */
                if ((pObj->createArgs.dumpDataType == NULL_LINK_COPY_TYPE_BITSTREAM_FILE)
                    &&
                   (queId == 0))
                {
                    for (bufId = 0; bufId < bufList.numBuf; bufId++)
                    {
                      chNum = bufList.buffers[bufId]->chNum;
                      OSA_assert (chNum < SYSTEM_MAX_CH_PER_OUT_QUE);
                      bitstreamBuf = ((System_BitstreamBuffer *)bufList.buffers[bufId]->payload);
                      /* Cache invalidate required as CPU copy is used */
                      OSA_memCacheInv((UInt32)bitstreamBuf->bufAddr, bitstreamBuf->fillLength);
    
                      fwrite(bitstreamBuf->bufAddr, bitstreamBuf->fillLength, 1, pObj->fpDataStream[chNum]);
                    }
                }
    
                for (bufId = 0; bufId < bufList.numBuf; bufId++)
                {
                    pChInfo = \
                    &pObj->inQueInfo[queId].chInfo[bufList.buffers[bufId]->chNum];
    
                    if (NULL != pObj->createArgs.appCb)
                    {
                        pObj->createArgs.appCb(
                                        pChInfo,
                                        (Void*)bufList.buffers[bufId],
                                        pObj->createArgs.appCbArg);
                    }
                }
    
                System_putLinksEmptyBuffers(pInQueParams->prevLinkId,
                                           pInQueParams->prevLinkQueId, &bufList);
            }
    
        }
        return SYSTEM_LINK_STATUS_SOK;
    }
    
    /**
     *******************************************************************************
     *
     * \brief This function implements the following.
     *    Accepts commands for
     *     - Creating Null link
     *     - Arrival of new data
     *     - Deleting Null link
     * \param  pTsk [IN] Task Handle
     * \param  pMsg [IN] Message Handle
     *
     *******************************************************************************
     */
    Int32 NullLink_tskMain(struct OSA_TskHndl * pTsk, OSA_MsgHndl * pMsg, UInt32 curState)
    {
        UInt32 cmd = OSA_msgGetCmd(pMsg);
        Bool ackMsg, done;
        Int32 chId, status = SYSTEM_LINK_STATUS_SOK;
        NullLink_Obj *pObj = (NullLink_Obj *) pTsk->appData;
    
        if (cmd != SYSTEM_CMD_CREATE)
        {
            OSA_tskAckOrFreeMsg(pMsg, SYSTEM_LINK_STATUS_EFAIL);
            return SYSTEM_LINK_STATUS_EFAIL;
        }
    
        status = NullLink_drvCreate(pObj, OSA_msgGetPrm(pMsg));
    
        OSA_tskAckOrFreeMsg(pMsg, status);
    
        if (status != SYSTEM_LINK_STATUS_SOK)
            return status;
    
        done = FALSE;
        ackMsg = FALSE;
    
        while (!done)
        {
            status = OSA_tskWaitMsg(pTsk, &pMsg);
            if (status != OSA_SOK)
                break;
    
            cmd = OSA_msgGetCmd(pMsg);
    
            switch (cmd)
            {
                case SYSTEM_CMD_START:
                    OSA_tskAckOrFreeMsg(pMsg, status);
                    if (pObj->createArgs.dumpDataType == NULL_LINK_COPY_TYPE_BITSTREAM_FILE)
                    {
                       /* File Write enabled for channels only from first inputQ (Q0) */
                       for (chId=0; chId<pObj->inQueInfo[0].numCh; chId++)
                       {
                         Vps_printf(" NULL LINK: Opening file for Dump \n");
                         pObj->fpDataStream[chId] = fopen((char *)pObj->createArgs.nameDataFile[chId], "wb");
                         OSA_assert(pObj->fpDataStream[chId] != NULL);
                         Vps_printf(" NULL LINK: Opened file for Dump \n");
                       }
                    }
                    break;
                case SYSTEM_CMD_STOP:
                    OSA_tskAckOrFreeMsg(pMsg, status);
                    if (pObj->createArgs.dumpDataType == NULL_LINK_COPY_TYPE_BITSTREAM_FILE)
                    {
                       for (chId=0; chId<pObj->inQueInfo[0].numCh; chId++)
                       {
                         Vps_printf(" NULL LINK: Closing Dump file \n");
                         if(pObj->fpDataStream[chId])
                         {
                             fflush(pObj->fpDataStream[chId]);
                             fclose(pObj->fpDataStream[chId]);
                         }
                         Vps_printf(" NULL LINK: Closed dump file \n");
                       }
                    }
                    break;
                case SYSTEM_CMD_DELETE:
                    done = TRUE;
                    ackMsg = TRUE;
                    break;
                case SYSTEM_CMD_NEW_DATA:
                    OSA_tskAckOrFreeMsg(pMsg, status);
    
                    NullLink_drvProcessFrames(pObj);
                    break;
                default:
                    OSA_tskAckOrFreeMsg(pMsg, status);
                    break;
            }
        }
    
        if (ackMsg && pMsg != NULL)
            OSA_tskAckOrFreeMsg(pMsg, status);
    
        return status;
    }
    
    /**
     *******************************************************************************
     *
     * \brief Init function for Null link. This function does the following for each
     *   Null link,
     *  - Creates a task for the link
     *  - Registers this link with the system
     *
     * \return  SYSTEM_LINK_STATUS_SOK
     *
     *******************************************************************************
     */
    
    Int32 NullLink_init(void)
    {
        Int32 status;
        System_LinkObj linkObj;
        UInt32 nullId;
        NullLink_Obj *pObj;
        UInt32 procId = System_getSelfProcId();
    
        for (nullId = 0; nullId < NULL_LINK_OBJ_MAX; nullId++)
        {
            pObj = &gNullLink_obj[nullId];
    
            memset(pObj, 0, sizeof(*pObj));
    
            pObj->tskId = SYSTEM_MAKE_LINK_ID(procId,
                                              SYSTEM_LINK_ID_NULL_0 + nullId);
            memset(&linkObj, 0, sizeof(linkObj));
            linkObj.pTsk = &pObj->tsk;
            linkObj.linkGetFullBuffers= NULL;
            linkObj.linkPutEmptyBuffers= NULL;
            linkObj.getLinkInfo = NULL;
    
            System_registerLink(pObj->tskId, &linkObj);
    
            /*
             * Create link task, task remains in IDLE state.
             * ipcOutLink_tskMain is called when a message command is received.
             */
            snprintf(pObj->tskName, 32, "NULL_%u", (unsigned int)nullId);
            status = OSA_tskCreate(&pObj->tsk,
                                   NullLink_tskMain,
                                   NULL_LINK_TSK_PRI,
                                   NULL_LINK_TSK_STACK_SIZE,
                                   0,
                                   pObj,
                                   pObj->tskName);
            OSA_assert(status == OSA_SOK);
            Vps_printf(" %s : Init done - linkid-0x%x\n", pObj->tskName, pObj->tskId);
    
        }
    
        return status;
    }
    
    /**
     *******************************************************************************
     *
     * \brief De-init function for Null link. This function de-registers this link
     *  from the system
     *
     * \return  SYSTEM_LINK_STATUS_SOK
     *
     *******************************************************************************
     */
    Int32 NullLink_deInit(void)
    {
        UInt32 nullId;
    
        for (nullId = 0; nullId < NULL_LINK_OBJ_MAX; nullId++)
        {
            OSA_tskDelete(&gNullLink_obj[nullId].tsk);
            Vps_printf(" %s : DeInit done - linkid-0x%x\n",
                gNullLink_obj[nullId].tskName, gNullLink_obj[nullId].tskId);
        }
        return SYSTEM_LINK_STATUS_SOK;
    }
    

  • Hello Vijay,

    Thanks for sharing source file as well as SDK info.

    I could see the change between TI VSDK3.0 and what you have. Basically NULL_LINK_COPY_TYPE_BITSTREAM_FILE has renamed to NULL_LINK_COPY_TYPE_BITSTREAM_FILE without any other changes.

    So you should be able to use NULL_LINK_COPY_TYPE_BITSTREAM_FILE. But again as you have RAW video data bitstream file type can't be used.

    I see two options
    1. Port support for RAW data from the vision_sdk\links_fw\src\rtos\links_common\null
    2. Add decode link in your current use-case and use NULL_LINK_COPY_TYPE_BITSTREAM_FILE with current NULL link.

    You use-case will look like below. Refer to "vision_sdk\apps\src\hlos\adas\src\usecases\null_src_decode_display\chains_nullSrc_Display.c" for decode configuration parameters.

    Capture -> Dup -> Display_Video

    Dup ->decode->Null

    GrpxSrc -> Display_Grpx

  • Hello Prasad,
    Thank you for the answer.I used option 2 and I was able to store the video data.

    Best Regards,
    Vijay