So after passing an article to my optical engineer I noticed either the diagram or the illustration of TRP angles is either not correct or confusing.
This is what I mean:
"DLP TRP pixel architecture utilizes square pixels and tilts by 17°. The mirror first tilts by 12° along the hinge then rolls by 12° to either ON or OFF position, resulting in a compound 17° angle."
Then there's this illustration on this page:
It looks like in the illustration the micromirror has rotated 12 degrees in one axis and 90 in the other?