Hello,
We intend to use the DLP NIRscan Nano EVM for transmittance measurements of solid samples. To that end, we are considering two options:
1) Use a reflective surface in front of the window and place the sample between the first condenser lens and the input slit.
2) Use an external IR source instead of the built-in lamps. In this case, it would be better to collimate the source light so that the sample is properly illuminated. However, we have to couple the light to the spectrometer.
Which one is the best approach? What are the optical parameters of the input stage (condenser lens)?
Thank you in advance.