This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J6 GPIO pin numbering



I am trying to build a cable from the GPIO out (J6) to the trigger in. The user guide gives a description of the function of each pin, but does not explain the pin ordering. Is the following J6 pin layout correct (assuming that the board is oriented with the printed writing and the projection direction facing up)?

^^^^^^^^^^^^^^^^^^^^^^^up^^^^^^^^^^^^^^^^^^^^^


01 02 03 04 05 06 07 08 09 10 11 12 13 14

15 16 17 18 19 20 21 22 23 24 25 26 27 28

Thank you for your help!