I am using the Firefly Camera instead of the Flea3 camera, and when I run the "DLP_LightCrafter_4500_3D_Scan_Application.exe" I get the following error:
Connecting to projector...
Configuring projector...
Connecting to camera...
Configuring camera...
Camera setup FAILED!
ERRORS: 2 and WARNINGS: 0
ERROR: PG_FLYCAP_C_SET_FORMAT_7_FAILED
ERROR: CAMERA_NOT_SETUP
I am not sure what I need to do so that the program recognizes that I am using the FIrefly instead of the Flea3 camera.