Hi,
The following led to the DLP lightcrafter 3000 shutting down after the boot menu completes:
I downloaded the latest software bundle 3.0 from the website. I then tried to upgrade the DM365 through an SD card. I had previously used this SD card for upgrades and had no problems. This time, once the DLP completed booting through the SD card, the LED flashed green and everything was ok. Then I switched the switch away from the SD card (back to ON) and when I connected the power, the DLP turned off after the booting screen completed (no colored bars).
After the DLP shuts down, a blinking red LED near the power connection (on the lower board) started flashing. The red LED stays on for about 5 or 6 seconds, turns off for under a second and then flashes. I don't know if there is any relation between the attempt to upgrade and this problem. Can you please help me figure out how to overcome this issue? Is the power a possible source of the problem?
Thanks,
Parmiss