Hi,
As Xinyi Fan described in his post (http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/850/t/358368.aspx), I cannot connect the DLP LIGHTCRAFTER anymore.
I could control the lightcrafter 3000 to project static images, but recently it can't be connected. The device can boot up and show the RGB stripes normally and can be recognized by the computer when it's connected via USB. However, It cannot be connected with the GUI provided. I checked the RNDIS network which is normal. I've tried both the XP and Win7 OS . It shows "connection error =5" in the windows XP OS. In the Win 7 OS, nothing is shown. It just cannot be connected.
Please help me with it.
Regards,
Zhenyue Chen