Part Number: DLP2010
Other Parts Discussed in Thread: DLPA2000, DLPC3430, DLPC3470, DLPC3435, TIDA-00325
I was told not long ago that due to limitations in software or maybe hardware of the DLP2010 controller chip you can only run in monochrome 960 Hz mode (8 bit x 120 Hz) one of the LEDs, not all on, and you also can't run at 1440 Hz (24 bit x 120 Hz) in color sequential mode, even though that is how the full color 24 bit 120 Hz is achieved, by a fast series of monochrome frames.
After reading articles on the inner workings of DMDs I have this realization: if I need 960 Hz monochrome but with all LEDs on (whitelight), why not just power on the LEDs not via the DLPController chip but otherwise and just keep them on without modulating? From what I understand modulation is just there so the color sequential RGB can be achieved in full color mode, if you just need one color and monochrome you can have that color light source on all the time and have the micromirrors either deflect them from the projection lens and screen or direct them. For the same reason you can have all the LEDs on all the time and not controlled/modulated by the DLPController chip to get the white light deflected or directed by each micromirror to show or not show a monochrome pixel.
I believe this workaround should allow me to get a white monochrome frames from a DMD such as DLP2010 from my understanding how DMDs create pixels and what the whole purpose of modulating the LEDs is.
Still I would like someone who has a professional knowledge on how DMDs work exactly to verify this theory and my proposed workaround for achieving what I need not supported by the DLPController chip yet.